Issue
Defining a device name for each Network 8000 Microflo II controller is possible when it is configured under a GCM. When defining it via a Niagara R2 UNC station, using the ASD driver, it is not possible.
Environment
- Niagara R2 UNC station
- Network 8000 Microflo II controller
Cause
Not a supported feature in the ASD driver.
Resolution
Due to the maturity of the Microflo II product this is a feature that will not be incorporated into the ASD driver.