Issue
Can a Network 8000 Microzone II base from 1993 (part numbers MZ2A-105 or MZ2A-106) be used with a MNL-800 controller card (part number MNL-800-101)?
Environment
Network 8000, Microzone II
Cause
Product obsolescence
Resolution
The Microzone II base has been through a few revisions but nothing that would prevent the MNL-800 controller card from working with it. Most of the revisions had to do with improving the power transient protection. If this is not a concern, then just note that the terminations and terminal labels will be slightly different. Ensure all I/O is reading correctly before leaving the jobsite.
ENCL-MZ800-PAN & ENCL-MZ800-WALL are replacement part numbers for the MZ2A-105 or MZ2A-106.