Issue
CNT block in XBuilder Xenta 700 Menta is replaced by a PI block.
Environment
- Xenta Server
- Xenta 701, 711, 721, 731
- XBuilder
- Menta
Cause
Differences between the regular Menta and the XBuilder Menta for Xenta 700 programming.
Resolution
The CNT block is replaced by the PI (Pulse input) block in XBuilder Menta. In XBuilder, connect the PI to a Binary or universal input where the sensor type is set to counter.