Issue
In Niagara R2, some GxPages and control objects are going to be duplicated many times. Each page and object will have many links. Is there a quick way of linking objects instead of the time intensive way of manually linking each individually?
Environment
Niagara R2
Cause
Graphics programming tip
Resolution
The Bundle container along with composites are used to expose control logic properties to a GxPage. The properties, to be linked, would be composited for both the control objects and Gxpages. Composite involves assigning the same name to both the GxPage object property and the control object property that are being linked. Once composited objects properties have been named, it is simply a matter of clicking on the “Match” button in the Link Properties screen to complete the link. Objects with the same name are then automatically linked.
The procedure for linking objects using Bundles and Composites can be located in Niagara Standard Programming Reference document.
Note that only native