Issue
TAC TRV-S series Butterfly Valve Body requires replacement.
Product Line
Field Devices
Environment
TAC TRV-S series Butterfly Valve Body installations.
Cause
Obsolescence of TAC TRV-S series Butterfly Valve Body.
Resolution
- Replace TAC TRV-S series Butterfly Valve Body with S-E VF208W series Butterfly Valve Body.
- Replace TAC MB15 / MB30 Actuator with S-E MF20 / MF40 series Actuator as appropriate.
It should be noted that where a TAC TRV-S series Butterfly Valve Body is to be replaced by a S-E VF208W series Butterfly Valve Body the TAC Actuator fitted to the TAC TRV-S Butterfly Valve Body will not be suitable for reuse on the S-E VF208W.Buttterfly Valve Body.
TAC TRV-S series Butterfly Valves utilise TAC MB15 / MB30 series Actuators.
TAC MB15 / MB30 Actuators are not suitable for use on S-E VF208W series Butterfly Valve Bodies.
S-E VF208W series Butterfly Valve Bodies utilise S-E MF20 / MF40 series Actuators.
S-E MF20 / MF40 series Actuators are suitable for use on TAC TRV-S series Butterfly Valve Bodies, but then no linkage kit should be mounted.