How do you reset the Viconics VT7200, VT7300, & VT7600 LON series thermostats back to factory default values?

Issue

How do you reset the Viconics VT7200, VT7300, & VT7600 LON series thermostats back to factory default values?

Product Line

TAC I/A Series

Environment

Viconics VT7200, VT7300, VT7600

Cause

There's no button or command that sets the thermostat to its default parameter settings.

Resolution

Either set them manually or through the snvts available via a LON integration.  The Viconics Lon Integration Manual will help with identifying the proper snvts to use.