Issue
Not possible to filter alarms on priority using comma.
If alarms with priority 1 and 4 to 10 should be shown in the alarm window, it has been possible in earlier versions (before Vista 5.1.4) to write "1,4-10" in the filter for alarm priorities. Today it is not possible to use the comma. An error message saying "Invalid input, check values and syntax" will appear when closing the filter.
Product Line
TAC Vista
Environment
Vista Workstation 5.1.4
Cause
It is only the user interface which will not allow a comma.
Resolution
Use the raw dialog for filtering the alarm window instead.
- Hold down Ctrl+Shift and click on the filter button
- Change APPRIO.
Fixed in version 5.1.5.