Issue
Description of how the Bacnet TimeSync works
Environment
Windows OS XP-Vista versions
Cause
Description of how the Bacnet TimeSync works
Resolution
The Bacnet TimeSync that is available on the Time tab in a device editor will only send out a Bacnet UTC TimeSync message to the Bacnet IP controllers that are in the list. This is not a automatic function, but is available to use when integrating 3rd party controllers into our system.