Issue
Unbound signals in Webstation appear as offline.
Environment
TAC Vista Webstation 5.1.4 and prior
Cause
In Vista Workstation, unbound signals are ignored; but in Webstation, and unbound signal is treated as offline. This may result in a red X across the entire component if any binding is unbound. This is an inconsistency across the two platforms.
Resolution
- Make sure all signals are bound. Even if it's a binding that is not used for any display purpose (like a multi-bind .[OBJECT] binding for example).
- Any signals that are unbound and unnecessary should be removed from components.