Issue
No routers exist to complete logical path needed for monitoring and control.
Environment
LonMaker
NL220
Vista
LNS
Cause
When initially creating a multi-port router, the internal L-IP FT-1250 channel was designated as an existing FT-10 channel. The drawing was built and then couldn’t be commissioned due to the physical topology not matching the drawing.
Resolution
With no logical path for the controllers and you attempt to move them to another channel, you must first correctly define the router in the Visio drawing.