Issue
Neuron model version mismatch.
Environment
LonMaker
NL220
Vista
LNS
Cause
This error will be generated if you attempt to use the Load method to load an application image into a device that is incompatible with the devices system image.
Resolution
In this case, you need to upgrade the devices system image. Some devices support the LoadEx method, which automatically upgrades the system image before loading the application image if there are compatibility problems.