Issue
The specified LonMarkObject is not dynamic.
Environment
LonMaker
NL220
Vista
LNS
Cause
This exception may be thrown if you attempt to assign a network variable to a static LonMarkObject with the AssignNetworkVariable method, unassign a network variable from a static LonMarkObject with the UnassignNetworkVariable method, or delete a static LonMarkObject with the Remove method.
Resolution
You can determine if a LonMarkObject is dynamic or not by reading its IsDynamic property.