Issue
The short cut created during the installation of DMS OPRIF 11.6 for DCT will not function.
Environment
DMS OPRIF 11.6 running in a Windows OS.
Cause
Unknown.
Resolution
To work around this issue, run the DCT.BAT located in the DCT folder. The installed desktop short-cut should be modified by editing the installed short cut line “call c350dct” to “call dct.bat”.
To improve system performance when running DCT modify the DCT.BAT file in the DCT folder from “dctgl.exe %1 %2” to “start /low dctgl.exe %1 %2”.