Issue
Is SQL 2000 Server with SP4 compatible with 1.91 CyberStation
Environment
LAN
SQL2000 SP4
CyberStation
Cause
Is SQL 2000 Server with SP4 compatible with 1.91 CyberStation
Resolution
Yes SQL2000 Sp4 is compatible with CyberStation 1.91. See Exchange online for current Andover Continuum Compatibility Matrix