Issue
Cannot get a new B3-866-v controller to come online
Environment
Continuum
BACNet
MSTP device
Cause
Using a 250 Ohm terminator on the MSTP bus
Resolution
Replace 250 Ohm terminator with the correct 120 Ohm terminator on each end of the bus
If the b3 will still not come online and other controllers are, disconnect the mstp bus and wait 10 seconds and reconnect.