Xenta 555 graphics are not display when requested.

Issue

When a graphic is selected from the Xenta 555 menu structure,  the graphic opens, but only the close (X) button is shown.

Product Line

Satchwell MicroNet

Environment

Xenta 555

Micronet

Cause

The Java TM Runtime version is not correct.

Resolution

Update Java TM Runtime to the latest version. This can be downloaded from here.