Issue
How to convert a B4-920 to a BCX4040
Environment
- BACnet
- B4-920
- BCX4040
- CyberStation
Cause
How to convert a B4-920 to a BCX4040
Resolution
- ASCII export the B4-920 then modify the dump file to change from the B4-920 to the BCX4040.
- Delete the B4920 from both the Continuum view and the BACnet view in Continuum Explorer.
- Import the converted dump file into the system.
- Reload the new BCX and all it's child objects.
- Execute a Find New BACnet Device to pull all the devices back into the BACnet view.
- Execute a Send to DB on the BACnet side to pull all the objects in.
NOTE: Another option if you are running version 1.90 CyberStation or greater is to change the model number through the controller editor in Continuum Explorer.