Replacement of Satchwell AR Series 1 or AR Series 2 Rotary Actuator by MD Series Rotary Actuator due to obsolescence. (Actuator Selection)

Issue

Satchwell AR Series 1 or AR Series 2 Rotary Actuator requires replacement

Product Line

Field Devices

Environment

  • Satchwell AR Series 1 or AR Series 2 Rotary Actuators installed on Satchwell MB Series or MBF Series Rotary Shoe Valve Bodies
  • Actuator types: ARE, ARM, ARX

Cause

Obsolescence of Satchwell AR Series 1 or AR Series 2 Rotary Actuators

Resolution

Replace Satchwell AR Series 1 or AR Series 2 Rotary Actuators with appropriate MD Series Rotary Actuators and Linkage Kits selected from the following:

  1. Satchwell AR Series 1 or AR Series 2 Rotary Actuators installed on Satchwell MB Series Screwed Rotary Shoe Valve Bodies
    • ARE Series 1 = MD10A-24 + Linkage Kit 914-1071-000
    • ARE Series 2 = MD10A-24 + Linkage Kit 914-1071-000 
    • ARM Series 1 = MD10B-230 + Linkage Kit 914-1071-000
    • ARM Series 2 = MD10B-230 + Linkage Kit 914-1071-000 
    • ARX Series 1 = MD10B-24 + Linkage Kit 914-1071-000
    • ARX Series 2 = MD10B-24 + Linkage Kit 914-1071-000 

Note: Should the Satchwell AR Series Actuator include a wired Auxiliary Switch then the following Accessory should also be installed on the MD Actuator as appropriate:

  • MD – S1  One independent Mains Voltage rated changeover contact Auxiliary Switch
  • MD – S2  Two independent Mains Voltage rated changeover contact Auxiliary Switches 
     
  1. Satchwell AR Series 1 or AR Series 2 Rotary Actuators installed on Satchwell MBF Series Flanged Rotary Shoe Valve Bodies 
    • ARE Series 1 = MD20A-24 + Linkage Kit 914-1070-000
    • ARE Series 2 = MD20A-24 + Linkage Kit 914-1070-000 
    • ARM Series 1 = MD20B-230 + Linkage Kit 914-1070-000
    • ARM Series 2 = MD20B-230 + Linkage Kit 914-1070-000 
    • ARX Series 1 = MD20B-24 + Linkage Kit 914-1070-000
    • ARX Series 2 = MD20B-24 + Linkage Kit 914-1070-000

Note: Should the Satchwell AR Series Actuator include a wired Auxiliary Switch then the following Accessory should also be installed on the MD Actuator as appropriate:

  • MD – S1  One independent Mains Voltage rated changeover contact Auxiliary Switch
  • MD – S2  Two independent Mains Voltage rated changeover contact Auxiliary Switches