Issue
Go to templates folder
Drag Event Enrollment to controller to create a new event enrollment
It prompts for event notification and point reference and enrollment looks fine.
When alarm is tested the event notification does not work and indicates fault.
Environment
Continuum
BCX40xx
B3
B4920
Cause
A Send to Database was not performed on the controller in the BACnet side of the Continuum Object Tree.
Resolution
When objects are added or modified on the Infinity side of Continuum's Object Tree, the changes do not take affect in the controller until a Send to Database is performed on the controller from the BACnet portion of Continuum Explorer Object Tree.