Issue
When accessing the VEO group of an LCM or GCM with XPSI revision 4.1 Terminal Mode, the data is displayed normally for about 90 seconds before it starts to become garbled. The problem begins at the top line of the display and progresses from the top down, one line at a time.
The arrow keys are not operable, cannot move the cursor to select attributes.
Environment
XPSI rev 4.1, Windows XP SP3, Windows Vista Pro, Network 8000 GCM, Network 8000 LCM
Cause
Unknown
Resolution
A work-around is to use a different terminal emulator instead of XPSI revision 4.1; possible alternatives are HyperTerminal or PuTTy. PuTTY.exe can be downloaded at http://www.putty.org/. Select putty.exe for Windows on Intel x86.