Issue
Is it possible to use TAC Menta from a TAC Workstation remote?
Environment
TAC Vista Workstation remote 5.1.5
TAC Menta 5.1.5
Cause
A Workstation remote is meant to be used by the customer to manage the system and don't as a engineering tool.
If installing a workstation remote Menta is not installed.
Resolution
No it is not possible to use TAC Menta from a TAC Workstation remote.