Issue
The IC-GEN OPC server does not communicate with a third party OPC client across Ethernet.
Environment
Sigma
IC-GEN OPC (all versions)
Cause
The IC-GEN OPC only supports a local IP address configured in the gateway.txt file.
Resolution
The IC-GEN OPC server can only be connected to third party OPC clients located on the same PC.
For more information see Release Note, click here
An example using an EIB I/O server, click here