Issue
Cannot Open Graphics Error. "The operation was not performed"
Environment
Continuum 1.90
Windows XP
Cause
Continuum 1.90 Sp1 not installed.
Resolution
- Install Continuum 1.90 Sp1
- Install all hotfixes
- Save the old DLL files to another folder, then delete them in the Continuum folders after the system is updated