Issue
Cannot establish communications to Modbus RTU using BCX X-Driver on Comm2
Environment
BCX 4040
Modbus RTU
Cause
Configuration of BCX to communicate with Modbus RTU device
Resolution
This excerpt from the Modbus RTU guide describes the parameters to configure the X-driver for Modbus RTU communications using the BCX. Click Here