Warning
Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support Services for assistance.
Issue
After upgrading, it now asks for the security key when launching Continuum.
Product Line
Andover Continuum
Environment
Continuum
Cause
Continuum stand-alone is not working in Demo mode after upgrading.
Resolution
Completely uninstall Continuum and re-install using the following steps.
Warning: Incorrectly editing the registry may severely damage your system. At the very least, you should back up your current settings and any valued data on the computer before making changes to the registry.
- Go to Control Panel > Add or Remove Programs.
- Remove Continuum.
- Reboot the PC.
- Remove EPI Builder Run-Time.
- Reboot the PC.
- Remove Sentinel System Driver Installer if installed.
- Reboot the PC.
- Remove the Continuum entries in the registry using Regedit.
- Start > Run > regedit
- Browse to HKEY_LOCAL_MACHINE\SOFTWARE\Andover Controls.
- Select the "Andover Controls" key, right-click and select "Export" to backup the reg key.
- Select the "Andover Controls" key, right-click and select "Delete" to delete the reg key.
- Reboot PC.
- Install Continuum without a security key attached to the PC.
You should now be able to start Continuum in stand-alone demo mode.