In MNB-1000s with firmware Revision 1.50E, the Router Table can be viewed and / or reset without resetting the Plant Controller.

Issue

In MNB-1000s with firmware Revision 1.50E, the Router Table can be viewed and /or reset without resetting the Plant Controller. This allows users to clear table entries that could cause router problems, without needing to reset the MNB-1000.

Product Line

TAC I/A Series

Environment

I/A Series MNB-1000 (Plant Controller) with firmware Revision 1.50E, or later.

WorkPlace Tech Tool, Commissioning Tool (WPT CT) version 5.7.7

Cause

Product enhancement.

Resolution

To view or reset the Router Table, choose from the following procedures, depending on the version of firmware:

1. For MNB-1000s with Revision 1.50E, use a web browser to access the Plant Controller to view or clear its Routing Table. Click here to see the Release Notes for Revision 1.50E, for more details.

2. For MNB-1000s with Revision 1.510, use the WorkPlace Tech Tool Commissioning Tool, version 5.7.7. 

Go to the Device Properties, Diagnostics Tab, Router Table Information button. Click here to see the Release Notes for WPT 5.7.7, for further details.