Issue
Using Lon Tunnel with Lon Flow Balance Tool
Environment
Lon Flow Balance (MNL-FLOW-BAL) all versions
R2 Niagara Lon Tunnel Client
G3 Niagara Lon Tunnel Client
Cause
Not applicable
Resolution
No, the Lon Tunnel Application (Niagara Application Tunneling) is not compatible with the Lon Flow Balance Tool. A direct connection (PCMCIA card or USB Lon Adaptor) must be present between the Lon VAV controller and the Lon Flow Balance Application. Also, LON1 is the only adapter address supported.