Issue
A TGML script has stopped working since upgrading to Vista 5.1.5.
The string.split method is not able to identify the "^" character in Vista 5.1.5 TGML scripts.
Environment
TAC Graphics Editor TGML 1.1.5 (Vista 5.1.5)
Cause
Unknown.
Resolution
Use string.split("\\^") instead. This may also apply to other characters but this has not been tested.