Issue
What are the fiber cabling specifications for an Infilink i2210?
Product Line
Andover Continuum
Environment
- Infinet Infilink i2210
- Mstp B-link-F Series
Cause
Fiber connections have specific parameters to work properly
Resolution
From the I2210 and B-link-F Series Installation Guides
- Fiber Optic cable: 62.5/125 duplex glass multimode fiber optic cable with ST-style connector
- Maximum attenuation allowable: 12 db
For some additional information related to fiber optic terminology, see the following: