Issue
A CX 9680 Netcontroller II does not provide access events to Cyberstation 1.80
Environment
Continuum Cyberstation 1.80
Cause
Incorrect firmware version
Resolution
Continuum Cyberstations versions 1.74 sp2 through 1.81, CX 9680 controllers will need to be at firmware version 2.000xxx
Continuum Cyberstations versions 1.82 through 1.9x, CX 9680 controllers will need to be at firmware version 2.100xxx
NOTE: Controllers are shipped with the latest firmware versions. If you are using Continuum Cyberstation 1.74sp2 - 1.81 you may need to down rev the firmware version.