Issue
Can you import a csv file to create infinity controllers.
Environment
CyberStation
Personnel Objects
CSV
Excel
Cause
To create objects in Continuum by importing a text file.
Resolution
A CSV import file can be used to create objects of most classes.
The CSV file must contain the at least three lines
- A line establishing the class of the objects that are to be created
- A header line describing the order of the attributes in subsequent lines with each attribute name separated by a comma.
- A line stating the value of each attribute separated by a comma.
If objects of more than one class are created a new section of the CSV file must be created beginning with the objects class.