Issue
How to interpret a M-Bus point details in a VX communication log such as External Temp [C] {1:0:0}.
Environment
Xenta Server 913
Cause
The External Temp [C] {1:0:0} message is providing important information about the point.
External Temp = Field Type
[C] = Unit
{1 = Storage #
:0: = Sub-Unit
0} = Tariff #
Resolution
Use the details of the communication log message to correct configuration problems in the device editor.
MVAL External Temp [C] {1:0:0} value not required
This message provides device details that a point exists, but the Device Editor is not looking for it.
!MVAL External Temp [C] {2:0:0} =not received
A point is expected but was not found.