Issue
BACnet MS/TP Bus Communication Troubleshooting Checklist
Product Line
TAC I/A Series
Environment
I/A Series BACnet controllers (MNB-70, MNB-V1, MNB-V2, MNB-300, MNB-1000) on an MS/TP bus.
Cause
BACnet MS/TP Bus Communication Troubleshooting Checklist
Resolution
This checklist provides several settings/configurations to review when faced with a communication problem at the controller level. The content was compiled from different resources, summarized, and laid out in an easy-to-use manner so as to provide a quick-reference document.