Issue
What is the maximum number of Network Controllers (InfinityController object) that I can have in my Continuum Database?
Environment
Continuum Cyberstation
Cause
Site expansion. What is the maximum number of Network Controllers (Netcontroller, ACX, etc...) that the system can grow too.
Resolution
There is no logical limit. Although you can only have up to 190 in one network folder. That is because the ACCNetID’s for controllers only go up to 190, after 190 controllers you will need to create a new Network object to house any new Network Controllers.