Issue
Integration of multiple Continuum databases.
Environment
Cyberstation
Cause
Unsupported configuration.
Resolution
DO NOT share a controller between databases, doing so will cause communications issues amongst others.
Alarms can be reported to the other 'sites' via email etc but integration within the Continuum system is not possible.