What is the replacement for a Drayton CRL 240 Actuator / Valve assembly.

Issue

The Drayton CRL 240 Actuator / Valve assembly is to be replaced.

Product Line

Field Devices

Environment

  • Replacement
  • Drayton
  • Actuator
  • Valve
  • CRL 240

Cause

The Drayton CRL 240 Actuator / Valve is obsolete

Resolution

The Drayton CRL 240 Actuator / Valve assembly is obsolete and there is no purpose built replacement.

The associated Drayton Valve Body was available in numerous sizes. 

These sizes are not available in current combined Actuator / Valve designs.

To replace one of the above Actuator / Valve Body combinations the following are required :-

  1. Valve sizes ½” – 2”
    1. Valve – MB(1/2" - 2")
    2. Actuator - MD10B-230 ( MD20B-230 could  be used if MD10B-230 is not available)
    3. Auxiliary Switch - MD-S1 ( MD-S2 could be used if MD-S1 is not available)
    4. Linkage Kit - LMD/AR-MB
  • Linkage Kit
  • Select S-E LMD/AR-MB Linkage Kit. (914-1071-000)
  1. Valve sizes 65mm – 100mm
    1. Valve – MBF(65mm – 100mm)
    2. Actuator – MD20B-230
    3. Auxiliary Switch - MD-S1 ( MD-S2 could be used if MD-S1 is not available)
    4. Linkage Kit - LMD/AR-MBF
  • Linkage Kit
  • Select S-E LMD/AR-MBF Linkage Kit. (914-1070-000)

To view the MB Valve Data Sheet, please click here.
To view the MD10B Actuator Data Sheet, please click here.
To view the MD-S1 Auxiliary Switch Data Sheet, please click here.
To view the LMD/AR-MB Linkage Kit Data Sheet, please click here.
To view the LMD/AR-MBF Linkage Kit Data Sheet, please click here.