How can a panel unit's title (description) be modified in a DMS database with OPRIF?

Issue

One of the Panel Units' title needs to be re-worded in a DMS database.  How is this done with OPRIF?

Product Line

TAC I/A Series

Environment

DMS 35, DMS 350A, DMS 3500

all revisions

Cause

Mechanical equipment naming has changed and the DMS database is being modified to match.

Resolution

The message text table lists the Panel Unit Descriptor Messages. 

Cursor down to the descriptor requiring modification and press the "=" key. 
Type in the new text and press Enter.

For more information, see Chapter 4 - "Setting Up Tables" in the DMS Operator Interface User's Guide (F-25467).