Issue
- When logging in once the login screen appears again
Environment
- Vista
- Webstation
- Windows 2003
- Windows 2008
Cause
Windows 2003 server and 2008 server have different default security settings for Internet Explorer and may deny cookies, this problem should not appear in Windows XP if default settings are used, you can also check if it works with Firefox, if it do so its ought to be the security settings in Internet Explorer.
Resolution
When the problem occurs, there should be a notification after the address bar. Click on that and allow an exception for the IP address for the Xenta.