Using Modbus RTU X Driver to connect to PM700 and PM750 Power meters.

Issue

Are examples available to show how to write Plain English programs and create points for a Modbus RTU X Driver linked to Schneider Electric Power meters?

Product Line

Andover Continuum

Environment

Modbus RTU X Driver

Schneider Electric PM700, PM750 Power meters.

Cause

Requirement for some examples to see how Modbus RTU programs can be written to poll for the data in a 3rd party Modbus device.

Resolution

The attached example was written by an application engineer in the UK to extract data from the Schneider Electric PM700 and PM750 meters.

This example provides the mapping of data for these 2 specific meters, but the polling principle utilized in the Plain English programming can be applied to any Modbus RTU interface

Download file here.