Issue
On an FTT-10 trunk segment wired in a Loop Topology, where should the LON-TERM1 terminator be installed? The Loop Topology is a subset of the Free Topology.
Environment
LonWorks FTT-10 network including I/A Series MNL controllers wired in a Loop Topology.
Cause
Installation detail
Resolution
In a Free Topology segment, only one termination (LON-TERM1) is required, and may be placed anywhere on the free topology segment.