Xenta webserver - SMTP settings

Issue

  • SMTP
  • Copy to
  • Blind copy to
  • Reply to

Product Line

TAC Vista

Environment

  • Vista
  • Xenta

Cause

In order to CC, BCC and the option to let a user reply to a sent alarm you need to configure the Xenta's SMTP settings

Resolution

There are 3 options under SMTP settings in Xbuilder

 

  • Copy to - The same as CC in outlook
  • Blind copy to - The same as BCC in outlook (A copy of the email sent discrete to chosen email)
  • Reply to - When a user gets an email about an alarm and clicks on reply, the address will become the same as the one specified here.