Issue
Get Error message "Error: Unable to create blueprint file" when trying to download to Xenta device
Environment
- TAC Vista
- Xenta 301
- Xenta 302
- Xenta 281
- Xenta 282
- Xenta 283
- Xenta 401
Cause
This can be caused if one or more of the I/O modules from the device does not have any subnet/node address defined.
Resolution
- Click on the Xenta in Workstation
- In the pane to the right double click on $IO
- Right click and select properties on the I/O modules
- Make sure that all modules have subnet node defined.