Issue
Multiple FLEXnet License File errors warn that the license file is about to expire or has already expired.
Errors may be logged in Windows system log that may look something like this:
(2372) Feature: Micronet.VisiSat.Core, expires on 30-apr-2011. This is a two week notice.
Multiple errors may pop up at once or may only occur daily.
Here are two examples of messages you might see.
Event Type: Warning
Event Source: taclic_LicenseServer
Event Category: FLEXnet License File
Event ID: 718
Date: 30/04/2011
Time: 12:00:52 AM
User: N/A
Computer: BMSSERVER
Description:
(2372) Feature: Micronet.VisiSat.Core, expires on 30-apr-2011. This is a two week notice
Event Type: Error
Event Source: taclic_LicenseServer
Event Category: FLEXnet License File
Event ID: 716
Date: 5/17/2012
Time: 2:55:15 PM
User: N/A
Computer: G15HVAC
Description:
(2516) This license (Vista.Server.LNS) has expired.
Environment
FLEXnet License Server
Cause
A valid site license and demo license have been left in the Vista license directory.
The system message is letting you know that the demo license will or has already expired.
Resolution
Remove or relocate the demo license once it is no longer required on site. This will prevent this error message from appearing in the Windows Event Viewer.