Issue
Change the path of acctrace .csv file
Environment
- Continuum
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
There are permission restrictions to the Continuum folder or there is a need to change the path to the acctrace .csv output file.
Resolution
If permissions are restricted to Continuum, you can change the path to this file. A good troubleshooting step is to send the file to c:\temp
When starting acctrace there is a field called "Filename for trace output:"
To change the path for the .csv file add the path in the field called "Filename for trace output:"
Ex. C:\Temp\ACCTrace_datetime.csv (leave the actual datetime that the program creates and only add the path C:\Temp ahead of the filename)
* On a Windows7 PC, the User Account Control changes the default path where files are created by ACCTrace. If Continuum is installed on the C drive, look in the following path for the trace file that is created:
c:\users\username\appdata\local\virtualstore\program files\continuum