Issue
Much of the literature being used for R2 and G3 reference the Niagara Jace model numbers. Is there a cross reference list available to cross Jace model numbers to UNC model numbers?
Environment
Niagara R2 and G3
Cause
The provided literature reference Jace model numbers.
Resolution
A cross of UNC to Jace controllers are as follow:
UNC-410-1 JACE-403
UNC-500-1 JACE-501
UNC-500-2 JACE-502
UNC-510-1 JACE-511
UNC-510-2 JACE-512
UNC-520-2 JACE-545
UNC-600-2 JACE-NP
UNC-610-2 JACE-NX
ENC-410-1 JACE-403-AX
ENC-520-2 JACE-545-AX
Tridium reference to Ax is Schneider Electric’s G3.