Issue
Is it possible to add a new font in the TGML graphics editor
Environment
Tac Vista 5.1.X TGML editor
Graphics Editor TGML 1.1.X
Cause
There are a number of reasons why a customer would like a particular font. For example, the customer has a corporate font that they use on their existing website and they would like to this to be used in their TGML graphics.
Resolution
To add a new font, just add the .ttf file to C:\Windows\Fonts (or the equivalent in your language) and restart TGML editor. Please be aware that the font must support regular (non bold) line weight, otherwise it will not be read by TGML editor at startup.