Issue
What is the procedure for upreving from 1.31 with MS Access to 1.93?
Product Line
Andover Continuum
Environment
CyberStation
Cause
No supported upgrade path when upgrading Continuum system that uses MS Access database to SQL database.
Resolution
Since there is no direct upgrade path the only option is to export everything to dump files from the old MS Access Continuum system then import into a new SQL ContinuumDB in new version of the CyberStation.
Graphics files from the old system are not compatible with new version of the Pinpoint Continuum application and will have to be discarded, although it may be possible to re-use bitmap files.