Can individual terminals be purchased for the MNL-10Rxx, MNL-15Rxx, or MNL-20Rxx controller?

Issue

Can individual terminals be purchased for the MNL-10Rxx, MNL-15Rxx, or MNL-20Rxx controller?

Product Line

TAC I/A Series

Environment

MNL controllers; MNL-10Rxx, MNL-15Rxx, or MNL-20Rxx

Cause

Replacement parts ...

Resolution

The individual terminals are not setup in the system for purchase.  The MNL-10Rxx, MNL-15Rxx, or MNL-20Rxx controller base assemblies are available for purchase under the following part numbers (MNL-BASE-100, MNL-BASE-150, MNL-BASE-200).