Issue
Windows 7 SP1 support for Continuum and Webclient.
Environment
Windows 7
Continuum v1.93 and above
Webclient v1.93 and above
Cause
Microsoft released Windows SP1 and it is not listed on the Continuum compatibility matrix.
Resolution
Continuum / WebClient v1.93
QA has not tested and qualified v1.93 for use with Windows 7 SP1. Microsoft Windows 7 SP1 was not released at the time of the Continuum 1.93 release.
Note: Some Partners and Branches have installed Windows 7 SP1 and have not reported any specific issues running Continuum or Webclient 1.93. Some PSS engineers are also running SP1 without issues.
Continuum / WebClient v1.94
QA has tested and qualified v1.94 for use with Windows 7 SP1. The note of this qualification was omitted from the Compatibility Matrix that was first released. The Matrix will be updated to reflect this new qualification for Continuum / WebClient v1.94.