Verifying Database returns Table Differences on a Server Client system

Issue

Verifying Database returns Table Differences on a Server Client system

Performing a database backup and restore is still functional.

Product Line

TAC I/NET

Environment

I/NET Seven

Server Client system

Server PC, DbCreate

Cause

When the I/O server is shut down before all of the client PCs some objects were opened and never closed. 

Resolution

  1. Restart I/NET on the Server PC
  2. Shut down I/NET on all the client PCs
  3. Shut down I/NET on the Server PC
  4. Use Db Create to Verify Database

NOTE: The Server Client configuration should only be used if you expect the Server to run 100% of the time.  If you wish to perform backups or other maintenance use the process above or use the tool found on the Buildings Business Community here.